The TIMER diagnostics is organized in the following structure
The analysis reports are listed in this folder.
This folder has the TIMER module diagnostics source code.
This folder has the header file for the TIMER diagnostics source code.